Archive of past news & events

The new CombiTac light housing with centralized locking

Specially developed for test applications that require high contact density.

MC4 – Now 1kV UL Recognized

Multi-Contact’s MC4 PV Connector is now rated for 1000 V UL and 1500 V TÜV*

Adjustable test probes with new tip shapes

IEC/EN 61010-031:2008 defines measurement categories for various working environments and defines the requirements for electrical test accessories. For the length of bare test probes, the norm requires a maximum of 4 mm...

Flex-Sol-Evo: New Lead Types for the Requirements of Tomorrow

In order to keep up with customer requirements in the cable area, and to cover forthcoming requirements, Multi-Contact AG has launched a selection of new leads called Flex-Sol-Evo. The Flex-Sol-Evo leads, which feature...

Increased Involvement in the Defense Industry

Multi-Contact AG is increasing its involvement in the defense industry and is poised to corner this market with its exceptional connection solutions. Whether on land, on the water, or in the air, the unique solutions...

Equipped for High-Speed Communication

Multi-Contact has upgraded its CombiTac modular connector system with a 10-Gbit module for Ethernet communication. The module complies with all CAT6A requirements. Like most products from the Multi-Contact selection,...

Link-H – the optional connection element for the high-performance MULTILAM LA-CUDD

Link-H, an optional application specially manufactured for the high-performance MULTILAM LA-CUDD, offers a number of advantages. Use of the Link-H allows an increase of 25% in the number of connection cycles. This...

Displaying results 1 to 7 out of 19